This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section.
| Name / View Group
Attribute ID Writable (W) Configurable (C) |
Attribute Description |
|---|---|
|
Latitude -- Setup 1041 W C |
Defines the angular distance, in decimal degrees, of the current location north or south of the equator. Lines of latitude are also known as parallels. The International standard defines north latitudes as positive values. |
|
Longitude -- Setup 1042 W C |
Defines the angular distance, in decimal degrees, of the current location east or west of the Prime Meridian. Lines of longitude are also known as meridians. The International standard defines east longitude as positive values. |
|
Offset -- Setup 956 W C |
Defines an offset to the computed Sunrise and Sunset times. The offset value is used to compute Present Value. A positive value makes the day longer and a negative value makes the day shorter. |
|
Periodic Update -- Setup 2192 W C |
Determines how often sun position and Present Value attributes update during normal operation. The default value is 5 minutes. |