Average Output Computation - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

In the case of binary types of input references, if the majority of inputs are at State 1 or the inputs are evenly split between State 1 and State 0, the Average output is commanded to State 1. If the majority of inputs are at State 0, the Average output is commanded to State 0.