Signal Select Attributes - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section.

Table 1. Signal Select Object Attributes
Name / View Group

Attribute ID Writable (W) Configurable (C)

Attribute Description

Input List -- Engineering Values

1062 W C

Contains the list of attribute references used in the Signal Select calculations. An analog type defined as a binary input is converted to a binary value prior to each computation, and vice versa.

Average Output -- Engineering Values

1063 W C

Specifies the object attribute whose value is updated using the calculated average of all of the inputs of the Signal Select Object.

High OR -- Engineering Values

1064 W C

Specifies the object attribute whose value is updated using the highest input of all the inputs in the Signal Select object, for analog point types. For binary point types, the value is updated using a logical OR condition of all inputs of the Signal Select object.

Low AND -- Engineering Values

1065 W C

Specifies the object attribute whose value is updated using the lowest input of all the inputs in the Signal Select object, for analog point types. For binary point types, the value is updated using a logical AND condition of all inputs of the Signal Select object.

Point Type -- Engineering Values

1173 W C

Specifies the type of input values monitored by the Signal Select object, the calculations it performs, and the outputs it produces. Point type can be analog or binary.

Failsoft -- Engineering Values

2567 W C

Routes to all the outputs if Setup is configured as Fail Soft. Fail Soft routes when the object becomes unreliable and when the output transitions from Reliable to Unreliable.

Setup -- Engineering Values

518 C

Defines whether the Fail Soft or Last Reliable value needs to be the output if the object becomes unreliable.

Execution Priority -- Execution

2197 W C

Indicates the relative importance of performing the function of the object within the device.