Object Interaction - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Different objects interact in an Optimal Start application. The following figure illustrates a sample Optimal Start application. The table describes the objects and their role in an Optimal Start application.

Figure 1. Optimal Start Object Interaction

Table 1. Optimal Start Application Object Interaction

#

Object or Attribute

Role

1

Optimal Start (OST) Object

Receives temperature, setpoint, and scheduling data to determine optimal start and optimal stop times for the building zone.

2

Schedule Object

Provides occupied and unoccupied times for the building zone.

3

Zone Occupancy Mode

Refers to the binary object (Binary Output, Binary Value, for example) that commands a zone to occupied or unoccupied. It is commanded by the Schedule object to occupied and by the Optimal Start to unoccupied, possibly earlier than scheduled if the Maximum Prestop Time attribute is non-zero.

4

Zone Warmup or Cooldown Mode

Refers to the binary object (Binary Output, Binary Value, for example) that commands the zone to warm up or cool down. It is commanded by the Optimal Start object at the optimal start time and released at the occupied time. It will not be released if the Zone Warmup or Cooldown (WC) Mode and the Zone Occupancy Mode objects are the same.

5-8

Zone Temperature,

Cooling Setpoint,

Heating Setpoint,

Outdoor Air Temperature

Refers to the analog attributes (within Analog Input objects, Analog Value objects, for example) that are referenced by the Optimal Start object and provide the temperatures and setpoints for use in calculations.