Global Data Sharing Object - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Menu Selection: Insert > Object > Global Data Sharing Object

The Global Data Sharing object provides a means for distributing information about changes in a single attribute value to other attribute reference points. This minimizes hardware costs and system complexity. For example, an NAE might have multiple AHUs on its network, but only one has an outdoor air sensor. The Global Data Sharing object can share the value from the single sensor with the other AHUs.

The data types defined for the Global Data Sharing object’s input and corresponding outputs should match. Otherwise, each output attempts to convert the value being received to the data type defined for it. The software does not check for data type consistency. Global data sharing is restricted to within one site.

For general information on Metasys system objects, see Common Object Attributes.