Demand Limiting/Load Rolling (DLLR) Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Menu Selection: Insert > Object > DLLR

The Demand Limiting feature helps you save money by limiting peak energy usage. The Load Rolling feature helps save money by reducing overall energy consumption. The DL portion of DLLR selectively turns off (sheds) equipment, such as fans and lights, or adjusts setpoints to limit energy use during peak times. The LR portion acts continuously to maintain a specified energy reduction by shedding unnecessary loads. A facility can implement either one or both of these strategies.

The DLLR object represents the attributes, commands, and reports that define the DLLR functionality. For information on the features and operation of DLLR, refer to the DLLR Technical Bulletin (LIT-12011288).