New User View - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Menu Selection: Insert > User View

Inserts a user navigation view (also referred to as user view, user-defined navigation tree, and user-defined tree) item into the All Items navigation tree. In online mode, the user view appears as a separate tab in addition to the All Items navigation tree if the user has permission for the user view. In online and offline modes, the user view appears in the User Views folder under the Site in the All Items tree.

Assign permissions to user views using the Security Administrator System in the online mode. You cannot assign permissions to user views in the SCT.

Tip: On the Configure screen, click the Configuration tab for further configuration.