Wireless Receiver Supervisor Object - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The Wireless Receiver Supervisor object is the root of the Wireless Sensor integration. The Wireless Sensor integration allows the NAE to communicate with the wireless sensing system over the Ethernet network. The Wireless sensing system consists of wireless receivers and wireless sensors.

Each integrated wireless field device (Wireless Receiver Object) and field point object (Wireless Sensor Object) appears under the Wireless Receiver Supervisor object in the Navigation Tree. Only one Wireless Receiver Supervisor object can be configured in each NAE or NIEx9.

Note: The Wireless Receiver Supervisor object is not available for network engines updated to Release 9.0.7 and later.