Multiple NIEs - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Migration can be split across multiple NIEs with the following constraints:

  • Only one N1 Migration object can exist per NIE per N1 network.

  • Multiple NIEs can reference the same N1 network.

  • Only one NCM object can exist per NCM per N1 Migration object.

  • Multiple NCM objects can reference the same NCM as long as they exist on different NIEs.

  • Only one point object can exist per NIE per N1 object.

  • Multiple point objects can reference the same N1 object as long as they exist on different NIEs.