Viewing User Graphics - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

To view user graphics, double click on or drag a graphic item from the Navigation Tree into the Panel Layout.

Note: To be sure the graphic item drops completely, release the drop with your cursor over the header section of the desired display frame.