Monitoring and Commanding Items Using Graphics in View Mode - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

Note: The Metasys system user interface provides the capability to monitor and command the Metasys system using graphics. To navigate through the system, see Navigating Graphics in View Mode.

To monitor your Metasys system using graphics:

Procedure

  1. Display graphics to show the status/state of your system components.
  2. Navigate through the system.
  3. To command objects/items using graphics, right-click on the symbol in View mode and select the desired command.

Results

Note: Right-clicking has no effect on Button Symbols.