Editing Text Blocks - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

About this task

To edit text:

Procedure

  1. With the selection pointer tool, double-click on the block. The block opens for editing.
  2. Change the text and click OK.
  3. To change the text properties, right click on the text block and select Properties from the menu.

Results

Note: You can change the font (type, size, bold, italic, bold italic), text color, background color, and border visibility/color.