Copying an Existing Graphic - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

About this task

Note: This is available when using the SCT only.

Procedure

  1. Click an existing graphic item in the Navigation Tree.
  2. On the Edit menu, select Copy.
  3. Click in the navigation tree where the new graphic is to appear.
  4. On the Edit menu, select Paste and name the new graphic.