Gauges: Analog Fill - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

To bind Analog Fill symbols to objects:

Procedure

  1. Double-click an Analog Fill Bar Graph icon. The Binding Information dialog box appears.
  2. Use the information in the following table to edit the fields.
    Table 1. Analog Fill Gauge Options

    Field

    Description

    Object

    Allows you to type in the Item Reference of the object you want to bind to the Analog Fill Gauge. Or, lets you click the Browse icon to launch a tree browser to select the object to bind to the Analog Fill Gauge.

    Attribute

    Allows you to select the object’s attribute to bind to the gauge.

    Fill Color

    Launches the fill color selector to select the color displayed by the bar graph.

    Orientation

    Chooses vertical or horizontal motion of the bar graph.

    High Limit

    Sets the high number for the display range of the gauge.

    Low Limit

    Sets the low number for the display range of the gauge.

    Units

    Displays the units used by the bound object.

    Status

    Displays the status of the object in the display box of the symbol.

    Properties

    Allows you to configure the text properties for the text in the display box of the gauge.

    OK

    Accepts changes.

    Cancel

    Cancels changes.