Dynamics: Switches - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

About this task

To bind Switch symbols to objects:

Procedure

  1. Double-click the Switch symbol. The Binding Information dialog box appears.
  2. Use the information in the following table to edit the fields.
    Table 1. Dynamic Switch Options

    Field

    Description

    Object

    Allows you to type in the Item Reference of the object you want to bind to the Switch. Or, lets you click the Browse icon to launch a tree browser to select the object to bind to the Switch.

    Attribute

    Allows you to select the object’s attribute to bind to the switch.

    Number of States

    Allows you to choose the number of states (2 or 3) the switch has.

    State 0/1/2

    Allows you to choose the text associated with each state.

    OK

    Accepts changes.

    Cancel

    Cancels changes.