Adding Text Blocks - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

To add text blocks in Edit mode:

Procedure

  1. Click the Text icon on the UGT Toolbar.
  2. Click the workspace to select a location for the text. The text block appears.
  3. Click the Select icon from the toolbar and double-click on the text block. The edit text box appears.
  4. Type in the text box and click OK.
  5. Select the Select icon on the UGT Toolbar.
  6. Select the text block and drag the sides to resize the block.