Edit Mode - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Edit mode is the mode used by the UGT to design and edit graphics. Access the Edit mode by clicking the Edit button on the UGT Toolbar. In Edit mode, you have access to all toolbar items/symbols and you can bind symbols to objects and link graphics to other graphics.

Right clicking in Edit mode brings up basic choices for editing graphics such as copy, paste, delete, duplicate, hide, and zoom, depending on the type of item you select. Double clicking in Edit mode brings up the binding information for a symbol.

For a list of mouse shortcuts, see the Mouse Shortcuts: Edit Mode topic.