Gauges Category - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Gauges provide an indication of the present value and status for the bound objects. If you select a single item or multiple items in the navigation tree and drag a gauge to the workspace, the UGT creates one gauge per item and binds each symbol to an item.

The following table lists the gauges included in the UGT.

Table 1. Gauges

Gauge Type

Symbol

Animation

Analog Fill Bar Graph

Bar moves to indicate value of bound object.

Dial Gauge

Dial needle moves to indicate value of bound object.