Graphic Workspace - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

When viewing an existing graphic or creating new graphics, the UGT runs in the Graphics Workspace, which is displayed in an active display panel. The background for the workspace defaults to a gray background. The graphic workspace displays all graphical symbols and a user-selectable Static Background. The UGT Toolbar shows only the appropriate tools for the UGT Modes the you are working in, either View Mode or Edit Mode.