Drag and Drop Shortcuts - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Consider the following shortcuts when dragging and dropping items to the Graphic Workspace:

  • If you select a Graphic Object in the navigation tree and then drag a button to the graphics workspace, the UGT creates a button already bound to the selected Graphic object.

  • If you select multiple field points in the Navigation Tree and drag a Value Display Box to the graphics workspace, the UGT creates multiple Value Display Boxes each bound to a field point.

  • If you select multiple field points in the navigation tree and drag a dynamic symbol or gauge to the graphics workspace, the UGT creates multiple symbols each bound to a field point.

  • If you select multiple field controllers along with a Graphic object in the navigation tree and drag a button to the graphics workspace, the UGT creates buttons for all the controllers. All buttons have the appropriate Alias string already entered.

  • To change the binding information for a symbol or to add binding information (if you drag and drop a symbol without selecting anything in the navigation tree), see Binding Symbols to Objects in Edit Mode.