Zoom Operations - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

You can zoom in the chart by holding down the mouse and sliding across the chart (either to the left or to the right). This action activates drag zoom. Zoom works for values on the x-axis, not values on the y-axis. To zoom out, click the Zoom Out link that appears in the upper right corner on a zoomed chart.

You can also zoom from the horizontal scroll bar by clicking and dragging on the ends of the scroll bar.