Trend Module Repositioning - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

You can reposition the trend module anywhere within the graphic’s display panel, but not across panels in a multiple-panel layout. To move the Trend Module, drag the title bar.

You can dock the Trend Module by dragging the module outside the panel boundary on the top, bottom, right or left side of the Metasys display panel. The Trend Module does not support multiple monitors.