Error Handling - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

If an error occurs while stored trend samples are retrieved (for example, the bound trend object does not exist or its supervisory device is offline), the chart line for this trend series does not appear. The error message Could not retrieve trend information appears as a tooltip for the existing legend item.