Behaviors - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Many elements of Graphics+ graphics support built-in or configurable behaviors.

Elements that support behaviors can flash if the bound object is in an alarm or warning state, change color based on the bound object's state or status, or show or hide depending on the bound object's state or status.

In the Metasys UI, the elements of the Graphics+ graphic display the behaviors as the bound object's state or status changes.

Note: Support of behaviors is limited in SCT.