Graphic Object - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The Graphics object defines the attributes that represent a defined user graphic for a given set of objects. Graphic objects must exist under a container object or under another Graphic object (this allows you to link graphics together).

For detailed information on the User Graphics Tool, refer to the User Graphics Tool section in the Metasys SMP Help (LIT-1201793).