Folder - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

A Folder object helps support the hierarchical organization of objects.

A total of 1000 objects can be added per folder, and up to 10 consecutive levels of Folder objects can be added within any other folder or object.

Note: You must name a new folder differently from the folders in the default set on the user interface.

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section.