Enable - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The Enable command allows the Schedule object to resume normal scheduling operation. The Schedule object starts the schedule as soon as it is enabled. When it is re-enabled, the Schedule object writes its current value to the scheduled items.