Prioritization - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Prioritization provides a means to ensure that alarms or event notifications with critical time considerations are not unnecessarily delayed. Priorities may be assigned To Offnormal, To Fault, and To Normal events individually within a notification class.