Multistate Input Attributes - Metasys - LIT-12011964 - MS-SCTRMOT-0 - MS-SCTSWO-0 - MS-SCTSWO-6 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

This object contains attributes common to many Metasys system objects. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Click the attribute name in the table for a description of the attribute.

Note: In the Notes and BACnet Notes columns, letters indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Object’s Reliability, W - Writable.
Table 1. Multistate Input Object Attributes - Focus/Configuration Tab

Attribute Name

Notes

BACnet Notes

Initial Value

Values/Options/Range

Description

Device Type

C,W

W

Null

Limit: 20 characters

Intrinsic Alarming Defined

C

Not Supported

False

False

True

Enables the BACnet Intrinsic Alarming feature in the object and the definition of related attributes.

Number of States

C,W

W

4

Minimum Value = 2

Maximum Value = 16

Out of Service

C,W

W

False

False

True

Present Value

D,N,R,W

D,N,R,W

 

States Text attribute identifies the value set for this attribute.

This attribute is required to be writable if Out of Service is True.

Reliability

W

W

 

No Fault Detected (Reliable), No Sensor, Over Range, Under Range, Open Loop, Shorted Loop, Multi State Fault, Unreliable Other Uses Reliability (Set 503).

State Text

       

States Text

C,W

C

Off Low

Med Hi

 

States Text Error Status

   

OK

Out of Memory: Indicates that memory overrun occurred while the system was adding custom enumeration for state text from the field device to the user dictionary.

OK: the addition of custom enumeration for state text from the field device to the user dictionary is successful, and state text from the device can be used.

Specifies the status of States Text on the supervisory device. This attribute cannot be archived or configured.

Status Flags

     

In Alarm, Fault, Overridden, Out of Service Uses BAC Status Flags (Set 9).

Use Remote Alarming

 

B,C,W

False