Lighting Output Attributes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab for this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Table 1. Lighting Output Object Attributes
Name / View Group

Attribute ID Writable (W) Configurable (C)

Attribute Description
Use Remote Alarming -- BACnet

853 W C

When the attribute Intrinsic Alarming Defined is set to True, determines where alarms for the object originate. If the remote integrated object contains attributes for originating alarms, then Use Remote Alarming defaults to True, causing the local mapper object to accept alarms from the remote integrated object that are routed to the network engine. If the remote integrated object does not contain attributes for originating alarms, then Use Remote Alarming defaults to False causing the local mapper object to originate alarms. When Use Remote Alarming is false, any alarms from the remote integrated object are ignored at the network engine. If the value of Use Remote Alarming is changed, a restart of the network engine may be required to assure correct operation. This attribute applies only to BACnet integrations.

Intrinsic Alarming Defined -- BACnet

569 W C

Enables the BACnet Intrinsic Alarming feature in the object and the definition of related attributes. For detailed information, refer to the BACnet Intrinsic Alarming section of the Metasys SMP Help (LIT-1201793).

User Name Is BACnet Obj Name -- BACnet

1092 W C

Controls whether the object’s User Name attribute is also the Object Name attribute. The Object Name attribute is not writable, so the only way to change the Object Name attribute is to edit the User Name attribute and set the User Name Is BACnet Obj Name attribute to True.