Lighting Output Object - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Menu Selection: Insert > Object > Lighting Output

The Lighting Output object allows a third-party BACnet workstation to represent a Lighting Output object in a BACnet field controller. The Lighting Output object represents in a linearized percentage the externally visible characteristics of a lighting output level. By adjusting the present value of this object, you can change the brightness level of banks of controlled lights. Typically, the adjustment value is from 5% to 85%.

User commands to the Lighting Output object provide special lighting-specific functions such as ramping, stepping, and fading. The lighting command also provides a blink-warn mechanism to notify room occupants that the lights are about to turn off. The blink-warning mechanism is internal to the Lighting Output object type and may cause a controlled set of lighting banks to blink on and off or issue a notification.