Life Safety Point Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The Life Safety Point object’s attributes represent the state of smoke detectors, fire detectors, security alarms, and similar devices. As a Life Safety Point, the state of this object can be one of 24 states.

The Life Safety Point object is a standardized object that represents a BACnet Safety Point Object as defined in the 2008 BACnet specification.