Channel Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Menu Selection: Insert > Object > Channel

The Channel object allows a third-party BACnet workstation to represent a Channel object in a BACnet field controller. The Channel object allows for the efficient adjustment of lighting brightness values to multiple lighting controllers. For example, with the Channel object, you can create logic in a BACnet field controller to turn lights on based on the state of occupancy sensors provided by the BACnet-based lighting system.