Global Calendar Object Reference - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Specifies a globally referenced calendar (if any) used as the master calendar for the site. Specifying a global calendar allows a site to synchronize many calendars so that only a single calendar (master calendar) needs to be changed. If you are using calendar references, you usually set up field controllers that reference a calendar on the engine, and engines that reference a calendar on a single supervisory engine, which is designated as the master calendar.