Binary Value Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Menu Selection: Insert > Object > BV

BV objects have similar software characteristics and capabilities to a Binary Input Object; however, Binary Value objects are not associated with any physical hardware and are the result of a control process or operator entry. This object allows you to hold a binary value for other objects to reference. For example, an Interlock can reference and base its operation on a binary value such as duty/standby.

For general information on Metasys system objects, see Common Object Attributes.