NCM Commands - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The table below lists the command specific to the NCM Object.

Table 1. NCM Object Commands

Command Name

Number of Parameters

Command Description

Clear Statistics

0

Resets the statistics at the NCM. The Message Errors, Message Receives, and Message Transmits attributes reflect these statistics.