MS/TP Field Device Object - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

The MS/TP Field Device object is used to represent FEC family MS/TP devices on the MS/TP Field bus. The MS/TP Field Device object appears as a child of an MS/TP Field Bus Integration object.

Note: The Object Type for this object is labeled FEC Family BACnet Device in the software.