LON Controller Attributes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Note: In the Notes column, attributes marked with the letter C are configurable and attributes marked with the letter W are writable.
Table 1. LON Controller Object Attributes - Focus/Configuration Tab

Attribute Name

Notes

Initial Value

Description

Enabled

C,W

True

If True, allows integration between the Metasys system and the LON controller.

Graphic

C,W

  Indicates the graphic associated with the object.

Graphic Alias

C,W

 

Indicates a portion of the graphic’s item reference, up to and including the name of the folder containing this object or the controller containing this point.

Offline

 

False

Displays the offline or online status of connected hardware. The LonWorks network server updates this attribute value.

Present Value

 

Offline

Displays the communication status of the object.

XIF Present

    Indicates whether a XIF file matching this controller’s Program ID was found.
Table 2. LON Controller Object Attributes - Diagnostic Tab

Attribute Name

Notes

Initial Value

Description

Command Count

    Displays the total number of commands sent to this controller.

Error Log

 

NOERROR

Shows the error log according to the last standard LonWorks network Query Status message.

Lost Message

 

0

Shows the number messages lost according to the last standard LonWorks network Query Status message.

Missed Messages

    Shows the number messages missed according to the last standard LonWorks network Query Status message.

Neuron Model

 

Neuron_3150

Shows the Neuron model according to the last standard LonWorks network Query Status message.

Node State

    Shows the state of the node according to the last standard LonWorks network Query Status message.

Offline Poll Count

 

0

Displays the total number of times this controller was sent a poll while offline.

Receive Transaction Full

 

0

Shows the number of times the transaction full message appeared in the last standard LonWorks network Query Status message.

Reset Cause

 

Clear

Shows the cause of the last reset according to the last standard LonWorks network Query Status message.

Reset Date

    Contains the date stamp of the last local Neuron statistics reset command.

Reset Time

    Contains the time stamp of the last local Neuron statistics reset command.

Total Messages to Device

 

0

Displays the total number of messages sent to this controller.

Total Single Message Failures

 

0

Displays the total number of failures for single messages sent to this controller.

Transaction Timeouts

 

0

Shows the timeouts that appeared in the last standard LonWorks network Query Status message.

Transmit Errors

 

0

Shows the number of transmit errors that appeared in the last standard LonWorks network Query Status message.

Version Number

 

0

Shows the version number according to the last standard LonWorks network Query Status message.