IP Field Controller Object Attributes - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab and the Diagnostics tab. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Note: In the Notes column, attributes marked with the letter C are configurable, and attributes marked with the letter W are writable.
Table 1. IP Field Controller Object Attributes - Focus/Configuration Tab

Attribute Name

Notes

Initial Value

Description

Enabled

C,W

True

If True, allows integration between the Metasys system and the IP field controller.

Vendor Name

W

 

Identifies the manufacturer of the device.

Model Name

W

 

Indicates the product code for the device.

Fixed Boot Version

   

Indicates the version of the Boot code in the field device. The Boot code is responsible for loading the Main code.

Last Update Date

W

Unspecified

Indicates the date the device was last updated.

Last Upload Time

W

Unspecified

Indicates the time the device received the most recent upload.

Graphic

C,W

Object Name:

Reference:

Indicates the graphic associated with the object.

Graphic Alias

C,W

 

Indicates a portion of the graphic’s item reference, up to and including the name of the folder containing this object or the controller containing this point.