IP Field Controller Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The IP Field Controller object defines a standardized BACnet object with attributes that represent the external, visible characteristics of a device. Only one Device object exists in each IP Field Controller. The IP Field Controller object appears as a child of a BACnet Integration object.