BACnet Device Object Commands - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The following table lists the commands supported by the BACnet Device Object.

Table 1. BACnet Device Object Commands
Command Name Parameters Description

Rediscover Text Strings

None

Resets the States Text across a supervisory device by rediscovering text strings from all mapped BACnet objects.

Note: When the Rediscover Text Strings command is sent from the Site Director device UI to another supervisory device and the UI is running on the supervisory device, you must close and restart the UI on the supervisory device in order for the text to appear correctly.
Reset Field Device

Type: Cold Start or Warmstart

Password

Resets the BACnet device.

Sync Field Device Times

None

Sends a high-priority time synchronization command to child devices, based on the device mapper object's Manual Time Sync Type.