Updating an Object Labels Export File - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Procedure

  1. Open the exported file in Microsoft Excel.
  2. In the New Name column, enter new names for any objects that you want to update. If you leave a cell in the New Name column empty, the object is not relabeled.
  3. In the Description column, modify the existing description or enter a new description.
    Note: If you leave the New Name cell empty, an object's description field is not updated. To update an object's description without changing the object's name, copy the existing name to the New Name cell.
  4. Click File, then click Save.
  5. A dialog box appears warning that some features may be lost. Click Yes.