Use the Update Object Labels feature to update the display name and description attributes of the following objects in an archive:
- Equipment
- Spaces
- Controllers
- Controller templates
- Equipment definitions
You can export each category of objects to a file, edit the file in a spreadsheet application such as Microsoft Excel, and then import the file to update the archive. If you update an object's display name attribute, its FQR is not altered, and no references or object relationships are changed.