Configuring the Metasys UI with SCT Overviews - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English
Figure 1. Configuring New Sites with the Metasys UI

Figure 2. Configuring Existing Sites with the Metasys UI

Note: With Metasys UI Release 2.1, you can associate all graphic types in the Graphics Manager of Metasys UI Offline and Metasys UI. Refer to the Metasys® UI Offline Help (LIT-12012116) for more information.

For more information about room schedules, controller templates, and the Rapid Archive Field Controller wizard, see the Rapid Archive Creation section. For more information about associating graphics, see the Graphics Association section.