Add Metasys UI Objects - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

About this task

To import a Rapid Archive Schedule file to create a new site, see Creating an Archive with the Rapid Archive Feature and Room Schedules. To import a Rapid Archive Schedule file and add Metasys UI objects to an existing site, complete the following steps:

Procedure

  1. In the Rapid Archive Field Controller Wizard, click Add MUI Objects.
  2. Navigate to a Rapid Archive Schedule file that contains space and equipment information, then click Import.
    Note: You must save the Rapid Archive Schedule as a .csv file. See Defining Space Information in the Rapid Archive Schedule.
  3. SCT processes the Rapid Archive schedule, and identifies any errors.
    • If there are errors in the Rapid Archive Schedule, a message appears that describes the error. The SCT archive is not updated. You do not need to undo any changes, or restore the archive. Click OK, correct the errors in the Rapid Archive Schedule, and then import the file again.
    • If there are no errors, a message appears indicating that the import is successful. Click OK.

Results

If the spaces that you define in the Rapid Archive Schedule do not exist in the archive, they are created.