Importing Controller Templates - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Procedure

  1. Navigate to the SCT Controller Templates folder in the All Items tree.
  2. Open the Action menu and click Import Template.
  3. Browse to the file location of the template you are importing and select the file.
  4. Click Import. The Notice dialog box appears.
    Figure 1. Import Notice Dialog Box

    Note: Verify the equipment definition association after import. If the definition does not exist, the controller template's Definition Link could be referencing an unbound equipment definition.