Modifying Controller Templates with the Rapid Archive Field Controller wizard - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2
Metasys SCT: System Configuration Tool Help
- Product
- Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
- Document number
- LIT-12011964
- Version
- 13.2
- Revision date
- 2020-01-21
Procedure
-
Open the Rapid Archive Field Controller wizard.
-
Click Edit.
-
Select the Create Points check box and clear the
Create Metasys UI Spaces and Equipment check box.
-
Navigate to the controller you want to modify.
-
In the Controller Template column, click the drop-down arrow, and do one of the following:
- Select a different controller template. This selection removes the existing controller template and deletes associated points, including any extensions, and recreates the points indicated by the new template.
- Select the duplicate controller template of
the current template selection from drop-down menu. For example, if * vavsd is
currently listed, select vavsd (Figure 1).
This selection deletes all of the existing points under the controller and recreates
them based on the current state of the selected controller template.
Figure 1. Duplicate Controller Template Selection
-
Click Save.