Manually Adding Points to Controller Templates - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020
  1. Open the controller template from the All Items tree.
  2. Select the Point List tab and click Edit to enter edit mode. Edit mode allows you to add points, folders, alarm extensions, trend extensions, totalization extensions, and arrange points.
  3. Click the Add icon to add a new point row to the Point List.
    Note: If points already exist when you click the Add icon, a new instance based on the original point selected is created.
  4. Enter point information until all red box requirements have been fulfilled.
  5. Click Save.

To make additional manual edits to your point list, see Figure 1 for descriptions of all icon functions in the controller template window.