Assigning Controller Templates with the Rapid Archive Field Controller wizard - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

About this task

Users can assign controller templates to controllers using the Rapid Archive Field Controller wizard.

Procedure

  1. Open the Rapid Archive Field Controller wizard.
  2. Click Edit, then navigate to the controller you want to assign a template to.
  3. In the Controller Template column, click the drop-down arrow. The drop-down menu appears.
  4. Select the template you want to assign the controller.
  5. Repeat steps 3 and 4 for all controllers you want to assign controller templates to.
    Note: If a controller has an existing template assigned, an asterisk will appear to the left of the template name (Figure 1). Leave the current controller template selection in place to maintain the current point structure for the controller. To modify the template, see Modifying Controller Templates with the Rapid Archive Field Controller wizard.
    Figure 1. Existing Controller Template Selection
  6. Click Save.