Rapid Archive Creation - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Menu Selection: Facility > Rapid Archive

The Rapid Archive feature of SCT offers simplified configuration of the SMP/SCT navigation trees and the Metasys UI by leveraging CAF, room schedule, and point schedule files. The wizard uses room schedules, controller templates, and equipment definitions to mass create equipment, spaces, and serving relationships with one click.

The following information describes how you can use the Rapid Archive to create a new site. For information on using the Rapid Archive to update an existing site with space and equipment information, see Rapid Archive Merging.

If you are a Johnson Controls employee, you can view informational videos about Rapid Archive Creation on the uLearn site: https://jc.kzoplatform.com/containers/928995312607959016.